TJA1028T/5V0/20 Communication cannot function properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1028T/5V0/20 Communication cannot function properly

3,385 Views
gududexiaolu
Contributor I

At present, LIN is communicating normally, VBAT is 12V, VCC is 5V, LIN waveform is normal, EN is 5V, REST is 5V, TX is 5V. Why is RX 0V causing communication to fail? Please provide a solution.

 

@guoweisun   #TJA1028T/5V0/20

 

目前,LIN正常通讯,VBAT为12V,VCC为5V,LIN波形正常,EN为5V,REST为5V,TX为5V,RX为什么是0V导致通讯无法正常运行

0 Kudos
Reply
10 Replies

3,365 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear 善逸科技李 善逸科技李,

the reason could be, that the RXD pin is reporting remote wake-up. Please confirm if the RXD 0V is happening in Normal mode or in Standby/Sleep modes. 

JozefKozon_0-1736230174292.png

With Best Regards,

Jozef

0 Kudos
Reply

3,355 Views
gududexiaolu
Contributor I

May I ask if you can provide me with your email? I would like to communicate with you via instant messaging

0 Kudos
Reply

3,362 Views
gududexiaolu
Contributor I

Thank you for your answer RX is experiencing this situation in normal operating mode

0 Kudos
Reply

3,346 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Gududexiaolu,

thank you for confirmation of the operation level. I am sorry, we are not allowed to share email addresses. 

Please share your schematic with voltage levels and part values. 
Please connect an oscilloscope probes on the RXD and LIN pins and please share the scope with their waveform during the unwanted RXD 0V. To check if the LIN signal is not holding the RXD low with LIN dominant signal.
 
JozefKozon_3-1736234421061.png
Please check if the TXD pin is not held low for longer then tto(dom)TXD. If yes, then the TXD dominant time-out function is triggered and the transceiver is disabled. 
 
JozefKozon_4-1736234515127.png
Please disconnect the RXD pin from your MCU and check if it is still pulled low. Your MCU might drive the RXD pin unwantedly low.
 
With Best Regards,
Jozef
0 Kudos
Reply

3,323 Views
gududexiaolu
Contributor I

LIN waveform is normal, both RX and TX should be high at the same time, but the failure issue is that RX is low level
The circuit diagram is not convenient to display here. I have already sent it to your forum email, please check it

0 Kudos
Reply

3,316 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Gududexiaolu,

thank you for the schematic. I have only one comment. There is no need to have pull-up resistors on the TXD and RXD lines. The TXD pin has an internal pull-up resistor to VCC and the RXD is driven by the LIN level. Please try to remove to pull-up resistors. The pull-up resistors might cause overtemperature on the TJA1028, which result in transition to off mode.

JozefKozon_0-1736316487086.png

JozefKozon_3-1736316818376.png

Please download and refer to the AH1003, section 5 "Mode control".

JozefKozon_1-1736316703563.png

It is available in the TJA1028 product page, under the Secure files. 

JozefKozon_2-1736316740439.png

With Best Regards,

Jozef

0 Kudos
Reply

3,294 Views
gududexiaolu
Contributor I

What does it mean that adding a resistor to TX and RX can cause overheating abnormalities? Can you explain it in detail?

 

I am temporarily unable to open the security file you mentioned

0 Kudos
Reply

3,289 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Gududexiaolu,

please follow the datasheet and the application hints, and other documents. Everywhere the TXD and RXD pins are connected without external pull-up resistors. If you will use parallel external resistor to the internal resistor, it will lower overall resistance value, resulting in more current flowing in the component. We do not have any document for this, so I cannot confirm if this is the case or not, but using external resistors is not according to the documents. 

Please connect an oscilloscope probes on the RXD and LIN pins and please share the scope with their waveform during the unwanted RXD 0V. To check if the LIN signal is not holding the RXD low with LIN dominant signal.
JozefKozon_0-1736415630032.png 
 

 

Please disconnect the RXD pin from your MCU and check if it is still pulled low. Your MCU might drive the RXD pin unwantedly low.
 
With Best Regards,
Jozef
0 Kudos
Reply

3,218 Views
gududexiaolu
Contributor I

Thank you for your answer.

Under what circumstances will TX and RX power on faster than VCC?

0 Kudos
Reply

3,213 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Gududexiaolu,

could you please elaborate on your question? The VCC can be powered via the external pull-up resistors from RXD or TXD or both. 

With Best Regards,

Jozef

0 Kudos
Reply