TJA1020: LIN INTERFACE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1020: LIN INTERFACE

1,165件の閲覧回数
Sathyashree
Contributor I

Hi,

In our validation/prototyping design, we are using TJA1020 for LIN interface. We need to know about  how much battery voltage can be given to the transceiver TJA1020 and also in LIN bus side how much voltage to be provided with analyser. Can we use 5V for VBAT and also in LIN bus side. Kindly suggest us a LIN bus analyser for this interface and also the provide us the evaluation board schematic of this transceiver.

 

Thanks

S Sathya shree 

ラベル(1)
0 件の賞賛
返信
1 返信

1,156件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

TJA1020 can work under the VBAT = 5 to 27 V;

You can refer to  AN00093 for getting more info:

AN00093 TJA1020 LIN transceiver (nxp.com)

0 件の賞賛
返信