TJA1020: LIN INTERFACE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1020: LIN INTERFACE

1,162 Views
Sathyashree
Contributor I

Hi,

In our validation/prototyping design, we are using TJA1020 for LIN interface. We need to know about  how much battery voltage can be given to the transceiver TJA1020 and also in LIN bus side how much voltage to be provided with analyser. Can we use 5V for VBAT and also in LIN bus side. Kindly suggest us a LIN bus analyser for this interface and also the provide us the evaluation board schematic of this transceiver.

 

Thanks

S Sathya shree 

Labels (1)
0 Kudos
Reply
1 Reply

1,153 Views
guoweisun
NXP TechSupport
NXP TechSupport

TJA1020 can work under the VBAT = 5 to 27 V;

You can refer to  AN00093 for getting more info:

AN00093 TJA1020 LIN transceiver (nxp.com)

0 Kudos
Reply