TJA 1055 cannot remote wake up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA 1055 cannot remote wake up

1,947件の閲覧回数
rexoplans
Contributor III

Hello, I am trying to implement remote wake up with the TJA1055T/3z integrated circuit. After putting the integrated circuit into sleep(0-1) mode, I transition it to sleep(0-0) mode. When I attempt to send a CAN message, I cannot detect any change on the ERR pin, and my VECTOR device that I'm using encounters an error. What could be the reason for this? (I am supplying 5 volts to the VCC pin, and I have pull-up resistors on the ERR-RX-TX pins with power supplied to them as well). What steps should I follow to achieve remote wake-up

タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,938件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Yiğit,

please share your schematic with voltage levels and part values. How have you connected the INH pin?

With Best Regards,

Jozef

0 件の賞賛
返信

1,935件の閲覧回数
rexoplans
Contributor III
Right now, it wakes up while in the integrated go-to-sleep mode, but it doesn't wake up while in the sleep mode. The Inh pin is connected to a MOSFET, and when there is a change in the Inh pin, I detect it from the processor and change my states accordingly. Currently, it works fine in the go-to-sleep mode but not in the sleep mode
0 件の賞賛
返信

1,932件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Yiğit,

thank you for the additional information. Please share the schematic with voltage levels and part values. Also please share the scope from the CANH and CANL bus. If the remote wake-up pattern is correct. 

JozefKozon_0-1708416478546.png

With Best Regards,

Jozef