TEF8102 datapattern test error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TEF8102 datapattern test error

1,908 次查看
longfeiwang
Contributor III

We have produced a total of 20 boards(S32R274+TEF8102), but two of them will generate a datapattern test error as the temperature rises after working at room temperature, and they can still work normally when the board returns to room temperature.What would cause this error to occur?This seems to be an error in CSI2 transmitting data, but temperature changes especially room temperature shouldn't affect it.

0 项奖励
回复
3 回复数

1,897 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

but two of them will generate a datapattern test error as the temperature rises after working at room temperature

Could you be more specific here? Is microcontroller failing or the sensor, or data are corrupt from sensor or .... ?

Best regards,

Peter

0 项奖励
回复

1,875 次查看
longfeiwang
Contributor III

There is no fault on the MCU. The temperature of the dolphin reaches over 60 degrees after the device runs for a few minutes. After the device is powered on again, the data pattern test in the dolphin ism fails. After the device is powered off and left for a period of time, after the temperature of the dolphin is lowered, and then powered on again, the data pattern test in the dolphin ism can pass. After the temperature rises, there is a problem when data is transmitted from dolphin to MCU through mipi.

0 项奖励
回复

1,828 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you please share register readout of ISM?

Best regards,

Peter

0 项奖励
回复