Symphony Studio under Win XP and path separators

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Symphony Studio under Win XP and path separators

1,809 Views
schi
Contributor I
It seems as if there is a path separators issue within symphony studio: The build process through the eclipse interface seems to delete single backslash \ path separators while unix-style separators / work fine.
 
While this is strange for a windows environment, it is even worse as the browse feature generate path names with single backslashes, so manual editing is required...
 
Any solution out there?
0 Kudos
Reply
1 Reply

1,305 Views
RandallAiken
Contributor I
Apparently,  "\\"  also works.   Just browse and select your file, and then add an extra "\" to each path separator.   


Message Edited by RandallAiken on 2008-10-22 02:06 AM
0 Kudos
Reply