Swapping P/N on CBTL02043ABQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Swapping P/N on CBTL02043ABQ

858 Views
avihayf
Contributor I

Hey,

I'm using 2:1 Mux, P/N CBTL02043ABQ.

Due to layout difficulties, I want to swap between P & N signals in the "IN" side of the mux, and swap them again in the "OUT" side of the mux (to keep the correct polarity).

See example below: 

MUX IO SWAP.jpg

According to the datasheet, there are no active parts (i. e. Pull up / Pull down / OD / ...) inside the mux that prevent me from doing the swap.

Is it possible to use the mux this way (regarding it internal electrical implementation)?

Best regards,

Avihay.

0 Kudos
Reply
1 Reply

790 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Avihay,

Yes. P and N channel are symmetrical.

Best regards,

Tomas

0 Kudos
Reply