Spice model for BFU910F Transistor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Spice model for BFU910F Transistor

ソリューションへジャンプ
1,930件の閲覧回数
huiyanhuan
Contributor I

Hi, 

I would like to request for the Spice model file for BFU910F, could you please send it to my email address? 
Thank you.

0 件の賞賛
返信
1 解決策
1,699件の閲覧回数
LPP
NXP Employee
NXP Employee

Sorry, we have no spice model for the BFU910F, only ADS model for nonlinear simulations, for linear S-parameters are available.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,700件の閲覧回数
LPP
NXP Employee
NXP Employee

Sorry, we have no spice model for the BFU910F, only ADS model for nonlinear simulations, for linear S-parameters are available.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,699件の閲覧回数
mhu
Contributor I

Hi,

I also would have required a non linear model for spice or qucs for BFU910F.

In the TDS it is stated that a spice model based on Gummel-Poon model is avalaible from Q1 2015.

Does it mean the TDS is in inaccurate / not up-to-date ?

What would then be best way to simulate the DC operating point ?

Thanks,

Regards,

0 件の賞賛
返信