Single channel ABS SB0401 Monitoring Module Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Single channel ABS SB0401 Monitoring Module Issue

2,853 Views
dhanabharathi
Contributor III

Hello @nxp ,

I’m using the SB0401 Single-Channel ABS module IC with an NXP S32K31xEVB-Q48 MCU as the SPI master. I transmit the monitoring/module data once every 10 ms, but the SB0401 monitoring module appears to reset/restart repeatedly (about once every 50 ms). Along with this, my SPI “error count” increases on every SPI transfer.

Below are the setup and my specific questions.

HW/SW setup

  • MCU (SPI Master): S32K31xEVB-Q48 (S32K31x family)

  • Device: SB0401 (Single-Channel ABS module IC)

  • Interface: SPI (LPSPI) (DMA based transfers)

  • Periodic transmission: every 10 ms

  • Observed issue: SB0401 monitoring module reset/restart every ~50 ms (see attached logs)

Observed behavior

  • The error counter increments for every SPI byte/word transfer.

  • I read AR (seed) from SB0401 message 18 and calculate MR based on that AR.

  • Despite sending frames periodically, the SB0401 monitoring module resets/restarts.

Questions

  1. MR calculation vs AR (Message 18)

    • My error count increases on every SPI transfer.

    • I calculate MR using the AR value received from SB0401 message 18.

    • Is it expected that an error counter would increment on every transfer in this condition, or does it indicate MR/AR logic is incorrect?

    • Please confirm the correct MR computation flow/timing relative to AR (message 18) and any common pitfalls (e.g., using stale AR, wrong byte/bit extraction, timing window, counter alignment).

  2. ACK position when writing Message 0

    • If I write data into Message 0 at TxBuf[0], where should I check the acknowledgement?

    • Example: For a write in TxBuf[0], does the ACK appear in RxBuf[0] (same word) or in RxBuf[1] (next word)?

    • If there is a defined “ACK occurs in the following SPI word/frame” rule, please share the exact mapping.

  3. Reference SW / CDD driver

    • Is there any reference CDD / example driver for SB0401 (C source or AUTOSAR-style CDD integration) that can be shared for guidance?

    • If not shareable, can you recommend the official SB0401 software package / app note / reference implementation details to follow?

 

0 Kudos
Reply
6 Replies

2,639 Views
dhanabharathi
Contributor III

Hi @guoweisun 

   yeah ok.

    Company:  Ettiksoft technologies Pvt ltd.

    project:  Two-wheeler single channel ABS. 



0 Kudos
Reply

2,593 Views
guoweisun
NXP TechSupport
NXP TechSupport

This part doesn't have CDD or other software drive and the reference schematic also need customer sign NDA then share.

 

0 Kudos
Reply

2,590 Views
dhanabharathi
Contributor III

hello @guoweisun 

  ok.  Any other reference code is there, like this module behaviour. 

0 Kudos
Reply

2,584 Views
guoweisun
NXP TechSupport
NXP TechSupport

For the example code I can't post here, could you please submit ticket from case port?

Home

0 Kudos
Reply

2,588 Views
guoweisun
NXP TechSupport
NXP TechSupport

Let me check again for the reference code about this special part.

0 Kudos
Reply

2,651 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Is possible to show your company and project information here?

0 Kudos
Reply