Simple Gui Guider Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simple Gui Guider Question

1,561件の閲覧回数
GeoffW123
Contributor I

Hello 

Just downloaded and been experimenting with Gui Guider. Nice App, looks very impressive. However I want to use LVGL V8.x.x. It would appear that Gui Guider is outputting V7.x.x version code.

Have NXP plans to update Gui Guider to LVGL version 8.x.x,  and if so when is it estimated to be available ?  Thanks

0 件の賞賛
返信
2 返答(返信)

1,541件の閲覧回数
GeoffW123
Contributor I

Thanks for the reply. LVGL Version 8 has changed quite a bit from Version 7, so manually converting is not an quick or easy task.

If you can pass on that you have already had a user request to provide an option for version 8 output, it might encourage that work to be done.

Thanks

0 件の賞賛
返信

1,545件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @GeoffW123 ,

Yes, NXP will update this tool and LVGL library occasionally. But there isn't a fixed upgrade plan.

 

Regards,

Jing

0 件の賞賛
返信