Simple Gui Guider Question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simple Gui Guider Question

1,556 Views
GeoffW123
Contributor I

Hello 

Just downloaded and been experimenting with Gui Guider. Nice App, looks very impressive. However I want to use LVGL V8.x.x. It would appear that Gui Guider is outputting V7.x.x version code.

Have NXP plans to update Gui Guider to LVGL version 8.x.x,  and if so when is it estimated to be available ?  Thanks

0 Kudos
Reply
2 Replies

1,536 Views
GeoffW123
Contributor I

Thanks for the reply. LVGL Version 8 has changed quite a bit from Version 7, so manually converting is not an quick or easy task.

If you can pass on that you have already had a user request to provide an option for version 8 output, it might encourage that work to be done.

Thanks

0 Kudos
Reply

1,540 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @GeoffW123 ,

Yes, NXP will update this tool and LVGL library occasionally. But there isn't a fixed upgrade plan.

 

Regards,

Jing

0 Kudos
Reply