Set SCT_OUTn by software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set SCT_OUTn by software

939 Views
martinglueck
Contributor I

I have a question:

I have the following problem to solve on an LPC1549.

I have configured on SCT to count external event's.

Now, I need to set/clear an output based on the number of these external "events". so far, so easy. Using the MATCH function of the SCT_OUTn does what I expected.

But now I have the situation that I need to set the SCT_OUTn immedeatly to ONE and clear it after n "events".

Reading through the documentaion, I could not find a way how the achive this.....

Has one an idea how that could be done?

Thanks,

Martin

Tags (2)
0 Kudos
Reply
0 Replies