SWUpdate with quashfs on eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SWUpdate with quashfs on eMMC

915 Views
alanlow
Contributor II

Hi,

I managed to add swupdate to imx8mm-evk imx-linux system kernel 5.10.72 and use swupdate-scripts to generate the base image and update image. The images work for rootfs with ext2, ext3 and ext4. However, I need rootfs to use squashfs instead but seems like the swupdate-script does not support squashfs?

Would appreciate if you can provide some lights on creating the base image which rootfs is squashfs fstype for imx8mm.

Thanks!

 

0 Kudos
Reply
0 Replies