STM32U585 VDDIO2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

STM32U585 VDDIO2

1,545 Views
Ballimo
Contributor I

Hello Community,

I am using the STM32U585 in a design, and I have VDD at 3.3V and VDDIO2 at 1.8V. 

The 1.8V rail is supplied by a 3.3V to 1.8V voltage regulator. I connected the Enable of this voltage regulator to one of the STM32U585 I/O (this I/O isn't on the PG port, because PG port is supplied by VDDIO2). Do you foresee any problem with this setup? I mean the 3.3V will turn on at first, and then the STM32 will turn on the 1.8V regulator, which supply VDDIO2 rail. 

In the datasheet it is clear that, VDDIO2 and VDD are two independent supplies. I just want a confirmation, and if someone here has a similar implementation in a working design.

Thank you,

Ballimo

0 Kudos
Reply
1 Reply

1,539 Views
Alondra
NXP TechSupport
NXP TechSupport

STM32U585 does not belong to the NXP portfolio and belongs to STMicroelectronics, please contact them for further support.

I'm sorry for the inconvenience this may cause

Best regards

Tech support

0 Kudos
Reply