SPT3.1 input ADDR is the same as output ADDR?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPT3.1 input ADDR is the same as output ADDR?

跳至解决方案
1,064 次查看
Shi_test
Contributor III

S32R45:

When I compile sdk1.1.0——apps——offline:

Shi_test_0-1679985224858.png

input ADDR:0x8B000000

output ADDR:0x8B000000

I wonder why the output file is correct?

  • Why don't they cover each other?
标记 (1)
0 项奖励
回复
1 解答
1,045 次查看
UrikRodriguez
NXP Employee
NXP Employee

Hi @Shi_test,

What happens is that the RFFT is done "in place", so the input is saved in the address 0x8B000000, then it is processed and the output is saved in the same address.   

 

Saludos,

Urik

在原帖中查看解决方案

1 回复
1,046 次查看
UrikRodriguez
NXP Employee
NXP Employee

Hi @Shi_test,

What happens is that the RFFT is done "in place", so the input is saved in the address 0x8B000000, then it is processed and the output is saved in the same address.   

 

Saludos,

Urik