SPI Flash Write Status Register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Flash Write Status Register

1,153 Views
yogeshddave
Contributor II

Hi Team,

I have LS1012A Board having winbond spi flash. I am able to perform basic read (0B) operation.  (using sf read command)

But now I want to perform write operation status register 1. But same is not working with sf write directly. 

I went through documentation which suggest to enable write then perform write operation. But not able to locate any option through which we can provide 0x06 (write enable) OR 0x01(Write status register-1) command through mtd_debug or sf command line option. 

Can you please provide input for this request.

0 Kudos
Reply
0 Replies