SPI Boot Mode, MSC8156ADS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI Boot Mode, MSC8156ADS

2,993 次查看
warlord
Contributor I

How to prepare a boot image for SPI Flash, is there any howto??

0 项奖励
回复
5 回复数

2,657 次查看
AndrewinApps
Contributor IV

I have something written up that I have done - but nothing official.


Please see the zip file I'm attaching to this post (with the readme txt document included.

Please give it a try and let me know if you have any feedback. As it's not an official doc - I'm going to delete the attachment after you've confirmed receipt.

 

Regards

0 项奖励
回复

2,657 次查看
warlord
Contributor I

Andrew in Apps, I have downloaded the attachment, thank you. Unfortunately, I will be able to test it in two weeks. I have succedded in I2C-booting. Now I have flashed the same code to M25P64, switched proper BOOT Port (FPGA says: BOOT SPI). Turned free mode, but the leds are not blinking.. I wonder if there is something to do with SPI CS signal. GPIO20/GPIO24...

0 项奖励
回复

2,657 次查看
AndrewinApps
Contributor IV

Were you using the txt file you created and tested for the EPROM image?

 

If so - could you test using the files provided in the zip file instead?

The EPROM boot txt file contains header info and other iteams that are not used in the SPI boot file.

0 项奖励
回复

2,657 次查看
warlord
Contributor I

I have succedded in SPI booting! Using the I2CBoot.exe I put a key -n instead of -f, so I got an ASCII-HEX includable file with C-array. Then I took EEPROM_burner project ang corrected it to burn SPI Flash. 

0 项奖励
回复

2,657 次查看
AndrewinApps
Contributor IV

great, thanks for the update.

0 项奖励
回复