SPE point to point implementation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPE point to point implementation

2,181 次查看
SarRaj
Contributor I

Hi 

If i wanted to do a point to point connection i can use ADTJA1101-RMII (x2), S32K148EVB-Q176 (x2) right without using the gateway. 

I wanted to read some sensor data at one point and need to control some actuators at the other end through spe. 

标签 (1)
0 项奖励
回复
3 回复数

2,167 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

yes, it should be possible to do point to point communication with boards you have.

 

BR, Petr

0 项奖励
回复

2,161 次查看
SarRaj
Contributor I

thanks for the reply.

 

Do we have the code stack available for TCP/IP, MQTT, OPC etc. Can anyone tell me what are the stack available for the S32k148 evaluation board. I wanted to broadcast the data whatever I received through the SPE.

Thanks in advance 

 

标记 (1)
0 项奖励
回复

2,118 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

lwIP TCP/IP stack is available within S32 Design Studio SDK, see file:///C:/NXP/S32DS_ARM_v2.2/S32DS/software/S32SDK_S32K1xx_RTM_3.0.0/doc/html_S32K148/lwip_s32k148_...

 

BR, Petr

0 项奖励
回复