SPE point to point implementation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPE point to point implementation

2,174件の閲覧回数
SarRaj
Contributor I

Hi 

If i wanted to do a point to point connection i can use ADTJA1101-RMII (x2), S32K148EVB-Q176 (x2) right without using the gateway. 

I wanted to read some sensor data at one point and need to control some actuators at the other end through spe. 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,160件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

yes, it should be possible to do point to point communication with boards you have.

 

BR, Petr

0 件の賞賛
返信

2,154件の閲覧回数
SarRaj
Contributor I

thanks for the reply.

 

Do we have the code stack available for TCP/IP, MQTT, OPC etc. Can anyone tell me what are the stack available for the S32k148 evaluation board. I wanted to broadcast the data whatever I received through the SPE.

Thanks in advance 

 

タグ(1)
0 件の賞賛
返信

2,111件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

lwIP TCP/IP stack is available within S32 Design Studio SDK, see file:///C:/NXP/S32DS_ARM_v2.2/S32DS/software/S32SDK_S32K1xx_RTM_3.0.0/doc/html_S32K148/lwip_s32k148_...

 

BR, Petr

0 件の賞賛
返信