SDXC in LS1012AXN7EKB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDXC in LS1012AXN7EKB

1,802 Views
sowmiya_a
Contributor I

Hi,

LS1012AXN7EKB - Will this part support 128 GB of sd card (SDXC)
0 Kudos
Reply
4 Replies

1,794 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @sowmiya_a,

 

LS1012A is compatible with the SD memory card specification version 3.01 and supports the high-capacity SD memory card which means it will support SDXC.

 

Regards,

Mrudang Shelat

0 Kudos
Reply

1,789 Views
sowmiya_a
Contributor I
Hi @mrudangshelat-13 
Based on your response my understanding is that LS1012AXN7EKB can support 128 GB capacity SD card (SDXC). Is my understanding correct?

Regards
Sowmiya
0 Kudos
Reply

1,772 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport
Spoiler

Hi @sowmiya_a,

 

As per the LS1012A reference manual, it supports standard, high and extended capacity card types which means it will support upto 2TB.

 

For more information regarding SD memory card specification version 3.01, please refer to this link.

 

Regards,

Mrudang

0 Kudos
Reply

1,769 Views
sowmiya_a
Contributor I

Thanks for the confirmation @mrudangshelat-13 

0 Kudos
Reply