SDXC in LS1012AXN7EKB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDXC in LS1012AXN7EKB

1,804件の閲覧回数
sowmiya_a
Contributor I

Hi,

LS1012AXN7EKB - Will this part support 128 GB of sd card (SDXC)
0 件の賞賛
返信
4 返答(返信)

1,796件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @sowmiya_a,

 

LS1012A is compatible with the SD memory card specification version 3.01 and supports the high-capacity SD memory card which means it will support SDXC.

 

Regards,

Mrudang Shelat

0 件の賞賛
返信

1,791件の閲覧回数
sowmiya_a
Contributor I
Hi @mrudangshelat-13 
Based on your response my understanding is that LS1012AXN7EKB can support 128 GB capacity SD card (SDXC). Is my understanding correct?

Regards
Sowmiya
0 件の賞賛
返信

1,774件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport
スポイラ

Hi @sowmiya_a,

 

As per the LS1012A reference manual, it supports standard, high and extended capacity card types which means it will support upto 2TB.

 

For more information regarding SD memory card specification version 3.01, please refer to this link.

 

Regards,

Mrudang

0 件の賞賛
返信

1,771件の閲覧回数
sowmiya_a
Contributor I

Thanks for the confirmation @mrudangshelat-13 

0 件の賞賛
返信