SDRAM Address testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDRAM Address testing

2,614件の閲覧回数
queen245
Contributor I
Hi,
 
 Wanted to know the below:
 
I wanted to know..... How the address given by the processor, say 0xA0000000 is the memory mapped address of the sdram. And the SDRAM is a 32MB which is 16M x16 datalines. 
 
Now there are 24 address lines used... 13 (A0-A12) for Rows + 9 (A0 -A8) for columns + 2 for Banks (BA0,BA1)
 
now if i want to write to the 0xA0008000 location (meaning A15 is high) but there is no A15 address line connected.
hence i wanted to know which address lines would be high and low for accessing memory location 0xA0008000
 
Can someone help me with this?
 
2. also wanted to know... How can i test the SDRAM address lines with the help of JTAG.
 
Awai your reply.
 
Queen245
 
タグ(1)
0 件の賞賛
返信
1 返信

1,724件の閲覧回数
Rame
Contributor I
Hi Queen245,

The SDRAM is addressed  through column and  Row address seperately and it is handled by the SDRAM controller.  The Physical  address  0xA0008000 is given to SDRAM Controller and controller in turn issue the Row address(A0 -A12) and column address(A0-A8) in the clock after tRAS. Refer the data sheet for all the timing.

I beleive the above explanation helps you.