SDK Example Projects does not work for EVK1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK Example Projects does not work for EVK1050

2,454 Views
Sherlock987
Contributor I

We have purchased the new evalboard SCH30168 REV B1: MIMXRT1052DVL6B. With MCUXpresso I have imported several SDK Examples for board evkbimxrt1050. When running them, they always results into hardware fault. I have lost lots of time finding the actual problem. Then I noticed when I import evkmimxrt1050 instead, the projects can be run without problems. Shouldnt this board work with evkbimxrt1050 or did I do another mistake?

The origin idea is that I want to import Mongoose example. There NXP1050 examples are provided but they also have hardware fault similar to evkbimxrt1050 projects. What are the differences?

Thanks for your help.

0 Kudos
Reply
6 Replies

2,420 Views
Sherlock987
Contributor I

Hi @EdwinHz thanks for your reply.

It is the MIMXRT1050-EVKB.

MCUXpresso IDE v11.10.0 [Build 3148] [2024-07-03]

SDK Version 2.16.000, manifest version 3.14.0

 

Ideally I would need the lwip_tcpecho_freertos example projects for this evalboard.

best regards

Sherlock

0 Kudos
Reply

2,408 Views
Sherlock987
Contributor I
So I have updated everything for MCUXpresso as well the SDK. Then I reimported the SDK for the EVKBIMXRT1050 board but it seems none of the projects works for the new Evalboard. It seems that only works for EVKMIMXRT1050 (older template projects). Please also note that I have Removed/Used Resistor to set it up for QSPI (I am not using Hyperflash) as recommended in the manual. Are there more than this modification which I should take care of?
0 Kudos
Reply

2,400 Views
Sherlock987
Contributor I
I have now also modified to Hyperflash but with the same fault after uploading the same projects. We have several evalboards to quickly switch back to QSPI. I have no idea what I'm doing wrong here.
0 Kudos
Reply

2,297 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Sherlock987,

Are you making sure to change the BOOT_CFG pins to Hyper Flash/QSPI Flash accordingly? 

 

Screenshot 2025-02-28 115919.png

0 Kudos
Reply

2,440 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Sherlock987,

Could you please share with me the following information:

Did you purchase the MIMXRT1050-EVK or the MIMXRT1050-EVKB? What version of MCUXpresso and SDK are you currently using?

BR,
Edwin.

0 Kudos
Reply

2,336 Views
Sherlock987
Contributor I
any progress here so far?
0 Kudos
Reply