SC18IS602B Chip Select Function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC18IS602B Chip Select Function

1,617件の閲覧回数
shubhatr_23
Contributor I

 Hi,

I want to interface SC18IS602B with DAC AD5504. For this Chip Select has to toggle(low to high) after 16bits of data is transmitted. What is the behavior of Chip Select pin on SC18IS602B? Will it toggle from low to high after each data byte is transmitted or after all data bytes in the buffer (up to 200 bytes) are transmitted? There is no timing diagram given in the data sheet.

Thanks in advance.

pastedImage_6.pngpastedImage_5.png

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,554件の閲覧回数
shubhatr_23
Contributor I

Hi Thomas,

Thanks for the reply. It would be really helpful if you can share a timing diagram for the same.

Thanks.

0 件の賞賛
返信

1,554件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Shreya,

The SSx outputs on the SC18IS602B are all low-true. They all are high when idle and only one (the selected one) is low when transferring all the data - in your case 2 bytes. 

Best regards,

Tomas