SC18IM704 interrupts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC18IM704 interrupts

Jump to solution
2,717 Views
jj100126
Contributor I

Hello, I have a SC18IM704-EVB and I want to pair it with PCF8575, is there a way for the SC18 to accomodate the INT pin of the PCF? How does the host get the interrupt?

0 Kudos
Reply
1 Solution
2,689 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Joshua,

yes, that is correct. You need to poll for checking if the !INT was asserted low by reading the IOState register.

With Best Regards,

Jozef

View solution in original post

0 Kudos
Reply
3 Replies
2,708 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Joshua,

you can connect the !INT pin to one of the GPIOs pin in the SC18IM704. The GPIO pins are configured as inputs after reset. 

JozefKozon_0-1653567634125.png

You can make sure, that the used GPIO is set as input only by setting the PortConfx registers to 00 or 01.

JozefKozon_5-1653568371693.png

JozefKozon_1-1653567691836.png

JozefKozon_2-1653567727380.png

Then you by reading the IOState register of the GPIO pin, you can check if the !INT pin is asserted (LOW).

JozefKozon_3-1653567851782.png

JozefKozon_4-1653568149213.png

With Best Regards,

Jozef

 

 

2,704 Views
jj100126
Contributor I

i have thought of this as well, setting the GPIO as input, but how about on the host side? Should the host poll everytime for the input from the INT pin, and if there's one, the host then read the inputs from the PCF?

I am also thinking of ditching the INT pin and just let the host poll for the PCF inputs directly

0 Kudos
Reply
2,690 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Joshua,

yes, that is correct. You need to poll for checking if the !INT was asserted low by reading the IOState register.

With Best Regards,

Jozef

0 Kudos
Reply