SGTL5000XNAA3 whether it able to record audio through microphone while speaker is in use

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000XNAA3 whether it able to record audio through microphone while speaker is in use

776 Views
santhoshwaran
Contributor I

SGTL5000XNAA3 whether this part can able to record audio through microphone while speaker is in use(LINE_OUT) and is it capable to use live recording and playing in speaker at same time

0 Kudos
Reply
3 Replies

750 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope this response finds you well.

In this case, the SGTL5000 needs to be programmed to select the desired input and output signal. The proper way to set the MIC_IN to LINE_OUT route is as follows:

MIC_IN -> ADC -> DAP(optional) -> DAC -> LINEOUT

 

The following community post might be useful for you.

Routing ADC -> DAC in sgtl5000

 

Please let me know if this information helps.

Regards,

David

0 Kudos
Reply

718 Views
santhoshwaran
Contributor I

hence it is capable to do as well above mentioned ?
(SGTL5000XNAA3 whether it able to record audio through microphone while speaker is in use)

0 Kudos
Reply

712 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope this response finds you well.

Do you mean route the microphone input signal to the speakers? That is possible.

But, if you want to use the microphone input signal and at the same time using the LINE-IN (routed to the speakers), I am afraid that is not possible. The system cannot accept LINE-IN and MIC simultaneously.

Please use the following block diagram as a reference:

diazmarin09_0-1653588141318.png

 

Please let me know if this information helps.

Regards,

David

0 Kudos
Reply