SC18IM700IPW - Alternative

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC18IM700IPW - Alternative

1,155 Views
Monogoly
Contributor I

Hello,

Is SC18IM700IPW active status in terms of its production status? If not, is there any alternative, which have the same pin-out and package? 

Best regards,

Ramazan Yaman 

0 Kudos
Reply
1 Reply

1,151 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ramazan,

The SC18IM700IPW/S8HP is not recommended for new designs. 

The SC18IM704PW is its functional replacement with exception of:

  • New pinout
  • GPIO no longer has quasi bidirectional mode
  • Lower operating supply voltage level (1.71 V vs 2.4 V)
  • Temperature range of -40 to +105 °C vs -40 to +85 °C
  • Device is rotated 180 degrees in the tape pocket; pin 1 is now in Quadrant 1

Capture.JPGCapture.JPG

Best regards,

Tomas

0 Kudos
Reply