What is the default state of SP in CD1020?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the default state of SP in CD1020?

ソリューションへジャンプ
1,618件の閲覧回数
jingfang
Contributor IV

What is the default state of SP in CD1020?

Before SP ports and input ports are configured.

0 件の賞賛
返信
1 解決策
1,603件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Before SP ports and input ports are configured, the SP pin is tri-state, and the value of state of  SP depends on the voltage on the SP pin.

The default configure of the SP pin is Switch to Battery (SB). 

If the Voltage is <4V , the state should be  0-open switch.

If the voltage is >4V, the state should be 1-closed switch.

I hope this answers your question.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,604件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Before SP ports and input ports are configured, the SP pin is tri-state, and the value of state of  SP depends on the voltage on the SP pin.

The default configure of the SP pin is Switch to Battery (SB). 

If the Voltage is <4V , the state should be  0-open switch.

If the voltage is >4V, the state should be 1-closed switch.

I hope this answers your question.

Best regards,

Tomas

0 件の賞賛
返信
1,581件の閲覧回数
jingfang
Contributor IV

Thanks a lot~

How about SG ?

If  Voltage  = 12V, what is the state?

0 件の賞賛
返信
1,576件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

For SG pins, if the voltage is > 4V, the state is open (0). If the voltage is < 4V, the state is closed (1).

Best regards,

Tomas