SC18IM700IPW - Alternative

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC18IM700IPW - Alternative

1,154件の閲覧回数
Monogoly
Contributor I

Hello,

Is SC18IM700IPW active status in terms of its production status? If not, is there any alternative, which have the same pin-out and package? 

Best regards,

Ramazan Yaman 

0 件の賞賛
返信
1 返信

1,150件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ramazan,

The SC18IM700IPW/S8HP is not recommended for new designs. 

The SC18IM704PW is its functional replacement with exception of:

  • New pinout
  • GPIO no longer has quasi bidirectional mode
  • Lower operating supply voltage level (1.71 V vs 2.4 V)
  • Temperature range of -40 to +105 °C vs -40 to +85 °C
  • Device is rotated 180 degrees in the tape pocket; pin 1 is now in Quadrant 1

Capture.JPGCapture.JPG

Best regards,

Tomas

0 件の賞賛
返信