SC16IS762 ttySCx not found under /dev/ directory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC16IS762 ttySCx not found under /dev/ directory

3,424 Views
ccc1
Contributor I

Hi teams,

Questions

I have installed driver SC16IS7xx.ko under ubuntu 20.04 in Nvidia orin nx board.
However, I can't find any ttySCx serial port under /dev/tty* directory.
I have no idea about the cause of this case. I am not sure how the driver works to install the serial port to the /dev/ directory.

system log

ccc1_1-1710434798424.png

/dev/tty* list

ccc1_0-1710434292980.png

Device Tree setting

ccc1_2-1710434907397.png

Thank you.

 

 

0 Kudos
Reply
3 Replies

3,380 Views
ccc1
Contributor I

Hi David,

Thanks for your help.

Is it the only solution to solve my issue?
I have facing some issues when running ltib.

Thank you.

0 Kudos
Reply

3,278 Views
brandonskyways
Contributor I

Have you found a solution for this?  I have the exact same problem with a SC16IS752.  I have an Orin NX on Auvidea JNX42 carrier

0 Kudos
Reply

3,411 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello ccc1,

I hope all is great with you. Thank you for using the NXP communities.

In this case, I can share a Linux driver for the SC16IS750 (single channel UART) even if SC16IS752 (two channel UART),but they are similar.

Please review the file attached to this response, you may find the drivers for both the I2C interface and the SPI interface for the SC16IS750 device.

For hardware review please also refer to the attached schematic.

I hope this information helps.

Regards,

David

0 Kudos
Reply