SC16IS762 ttySCx not found under /dev/ directory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC16IS762 ttySCx not found under /dev/ directory

3,425件の閲覧回数
ccc1
Contributor I

Hi teams,

Questions

I have installed driver SC16IS7xx.ko under ubuntu 20.04 in Nvidia orin nx board.
However, I can't find any ttySCx serial port under /dev/tty* directory.
I have no idea about the cause of this case. I am not sure how the driver works to install the serial port to the /dev/ directory.

system log

ccc1_1-1710434798424.png

/dev/tty* list

ccc1_0-1710434292980.png

Device Tree setting

ccc1_2-1710434907397.png

Thank you.

 

 

0 件の賞賛
返信
3 返答(返信)

3,381件の閲覧回数
ccc1
Contributor I

Hi David,

Thanks for your help.

Is it the only solution to solve my issue?
I have facing some issues when running ltib.

Thank you.

0 件の賞賛
返信

3,279件の閲覧回数
brandonskyways
Contributor I

Have you found a solution for this?  I have the exact same problem with a SC16IS752.  I have an Orin NX on Auvidea JNX42 carrier

0 件の賞賛
返信

3,412件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello ccc1,

I hope all is great with you. Thank you for using the NXP communities.

In this case, I can share a Linux driver for the SC16IS750 (single channel UART) even if SC16IS752 (two channel UART),but they are similar.

Please review the file attached to this response, you may find the drivers for both the I2C interface and the SPI interface for the SC16IS750 device.

For hardware review please also refer to the attached schematic.

I hope this information helps.

Regards,

David

0 件の賞賛
返信