SC16IS760 maximum baud rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC16IS760 maximum baud rate

Jump to solution
2,458 Views
Martin10
Contributor I

Dear Sir/Madam,

Based on the datasheet of SC16IS760, it states that the maximum baud rate this part can generate is 5 Mbps. 

Also, from the datasheet I can see that the baud rate can be generated from the external crystal. I am wondering if there is a maximum crystal frequency that SC16IS760 can interface with? Would it work well with a 32 MHz crystal, just for example?

Thanks!

0 Kudos
Reply
1 Solution
2,442 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please see datasheet page50-Table 38. fXTAL dynamic characteristics

 

View solution in original post

3 Replies
2,437 Views
Martin10
Contributor I

I see. Thanks! 

 

Another question on the load capacitance for the crystal. In figure 16, it shows that the two load capacitors used are different in the capacitance. However, in the past I typically see crystals with two capacitors with equivalent value.

Any particular reason to use two different capacitors in figure 16? Thanks! 

0 Kudos
Reply
2,418 Views
guoweisun
NXP TechSupport
NXP TechSupport

No particular reason,you can use the same value.

 

2,443 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please see datasheet page50-Table 38. fXTAL dynamic characteristics