SC16IS760 maximum baud rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC16IS760 maximum baud rate

ソリューションへジャンプ
2,416件の閲覧回数
Martin10
Contributor I

Dear Sir/Madam,

Based on the datasheet of SC16IS760, it states that the maximum baud rate this part can generate is 5 Mbps. 

Also, from the datasheet I can see that the baud rate can be generated from the external crystal. I am wondering if there is a maximum crystal frequency that SC16IS760 can interface with? Would it work well with a 32 MHz crystal, just for example?

Thanks!

0 件の賞賛
返信
1 解決策
2,400件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please see datasheet page50-Table 38. fXTAL dynamic characteristics

 

元の投稿で解決策を見る

3 返答(返信)
2,395件の閲覧回数
Martin10
Contributor I

I see. Thanks! 

 

Another question on the load capacitance for the crystal. In figure 16, it shows that the two load capacitors used are different in the capacitance. However, in the past I typically see crystals with two capacitors with equivalent value.

Any particular reason to use two different capacitors in figure 16? Thanks! 

0 件の賞賛
返信
2,376件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

No particular reason,you can use the same value.

 

2,401件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please see datasheet page50-Table 38. fXTAL dynamic characteristics