SC16IS752IPW Reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC16IS752IPW Reset

1,180件の閲覧回数
Pudl
Contributor I

Hello together,

I use the SC16IS752IPW 16 times on a big PCB.

Since I made a new revision of the PCB the SC16IS752IPW allways looses its setting (makes a reset) after switching a relais near the chip. The astonishing thing is, that between the revision bevor and the actual one I din't change anything around the Relais or the  SC16IS752IPW.

Measuring the souroundings of the chip I get a ripple at the 3.3V supply voltage (400mVpp for 1us) at the Reset input (1Vpp for 100ns) and at the I²S Data/Clock (1Vpp for 100ns) while switching the Reliais. Can this be the reason for the reset of the chip?

Best regards

Michael Pfab

0 件の賞賛
返信
1 返信

1,082件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Michael Pfab,

Yes, I do believe that the cause of the reset you are seen is the ripple you are seen at the Reset input.

Suggest you to add a decoupling capacitor on this rail to try to reduce the ripple.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信