SC16IS750 - TX/RX disable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC16IS750 - TX/RX disable

1,437件の閲覧回数
robin_ptl
Contributor II

Hi,

I notice in table 10 of the datasheet that bits 2 and 1 of register address 0x0F allow "transmitter disable" and "receiver disable", can I verify the expected operation of these lines when disabled?

I was hoping that the TX and RX lines would be undriven and remain high impedance or at 0V.  In practice we're finding that the TX line is continuing to idle high (3.3V in our case). We're changing these bits in the register and are reading the register back correctly, confirming that the RX and TX disable bits have been changed from 0 to 1.  We do not have other devices or pull-up resistors connected to the line.

Thanks,

Robin

0 件の賞賛
返信
1 返信

1,378件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

You test result is correct, the TX is keeping high when your disable these function about this device.

0 件の賞賛
返信