SC16IS741A Rx (no FIFO) Tx (with FIFO)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC16IS741A Rx (no FIFO) Tx (with FIFO)

787件の閲覧回数
kenstewart-smit
Contributor I

Re: SC16IS741A

I need to interrupt on every Rx character (no Rx FIFO needed) but also need to be able to use the Tx FIFO so I don't have to wait for each Tx character.  Is this possible with the SC16IS741A and if so, what register (and register settings) do I need to use?

Thanks

タグ(1)
0 件の賞賛
返信
0 返答(返信)