SC16IS741A Rx (no FIFO) Tx (with FIFO)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SC16IS741A Rx (no FIFO) Tx (with FIFO)

782 次查看
kenstewart-smit
Contributor I

Re: SC16IS741A

I need to interrupt on every Rx character (no Rx FIFO needed) but also need to be able to use the Tx FIFO so I don't have to wait for each Tx character.  Is this possible with the SC16IS741A and if so, what register (and register settings) do I need to use?

Thanks

标记 (1)
0 项奖励
回复
0 回复数