SBC FS26 state Flow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SBC FS26 state Flow

Jump to solution
6,371 Views
Naveen158
Contributor II

Hello, its a bit difficult to understand the Simplified functional state diagram given in the datasheet of FS26 as somethings are not mentioned Detailly, is there any Documented or Video kind of thing where this is Explained detailly, if not Can someone Explain it in the Post.

 

 

1 Solution
6,348 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Naveen, 

I have sent you an email.

With Best Regards,

Jozef

View solution in original post

12 Replies
4,505 Views
agouda
Contributor II

Hello @JozefKozon ,

I have the Eval-Board RDK358BMU, and facing some issue with FS26 w.r.t Standby mode and wakeup. 

could you please send me the same document ?

would also appriciate if you send me an example, considering Eval-Board RDK358BMU.

B.T.W , my company has already a valid NDA.

thanks in advance

BR

Abdullah

0 Kudos
Reply
5,740 Views
Djuric
Contributor III

@JozefKozon Can you send me the same document?

My company has a valid NDA agreement with NXP.

Thank you.

0 Kudos
Reply
6,349 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Naveen, 

I have sent you an email.

With Best Regards,

Jozef

5,714 Views
Djuric
Contributor III

@JozefKozon I would appreciate it if you could send me the same FS26 diagram you mentioned in the previous comment. The company I work for has a signed NDA agreement with NXP, which I also uploaded via the NXP website. Thank you.

0 Kudos
Reply
5,697 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Djuric,

I apologize for a late reply. I have checked our NDA database and unfortunately I couldn't find your company listed there. If the NDA was signed only recently, it is possible that it wasn't entered into our system yet. Please create a new case here and we will support you via the case.

JozefKozon_0-1731045459509.png

I apologize for inconvenience and thank you for your understanding. 

With Best Regards,

Jozef

5,688 Views
Djuric
Contributor III

I opened a new ticket.
The only problem I can think of is that you entered the wrong name of the company I work for.
If you contact me by private message, I will send you the exact name of the company as well as the tag from the NDA contract.

This whole process is very slow and unnecessarily complex...

0 Kudos
Reply
5,681 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Djuric,

thank you for creating the case. I see it already in our inbox. We will support you via the case. For your company name, yes I have entered incorrect name. I have read your company name from your email address, but this is not correct one. In the case you created I see your company name in the description and for this, yes there is a valid NDA in our database.

With Best Regards,

Jozef

0 Kudos
Reply
5,546 Views
Djuric
Contributor III
@JozefKozon Could you do me a favor and send me an email with the requested FS26 diagram.
I would appreciate it very much.
0 Kudos
Reply
5,414 Views
Djuric
Contributor III

@JozefKozon Please send me this file.
It has already been established that there is a valid NDA agreement.
Thank you.

0 Kudos
Reply
6,148 Views
MVR
Contributor V

Hello @JozefKozon 

Can you please send me this file as well, please?

0 Kudos
Reply
6,328 Views
Naveen158
Contributor II

Hi Jozef,

Yeah, Just gone through the Application Note, things are somewhat clear in this.

Thank you for the Document.

6,344 Views
Naveen158
Contributor II

I am using FS26
Safety system basis chip with low power for ASIL D/ASIL B (ds616040-FS26) Datasheet, isn't it the same ?

0 Kudos
Reply