SBC Controller UJA1075A software-support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SBC Controller UJA1075A software-support

3,827 次查看
c_fischer
Contributor I

Hi, all !   I want to use a SBC Controller UJA1075A in a non-automotive solution. My question is, is there a little bit software-support for this part, for example a LIB-File or an INCLUDE File for C ?   Thanks. Claus

标记 (1)
5 回复数

3,344 次查看
vinicius_olivei
Contributor III

Hello everyone,

Did anyone manage to implement this SBC? Is it possible to share the code of function void SpiSend(unsigned int *tx) ?
I have some troubles to activate CAN 5V, for example I send 0x2C00 but nothing happens.

Is there any way to test if the communication is working properly?

Best.

0 项奖励
回复

3,344 次查看
c_fischer
Contributor I

Hello, Tomas,

Yeah! It's more, more than I expected. Thanks!

So I do not have to reinvent the bike.

I know, that such SBC's with combined LIN/LON receivers were designed especially for automotive applicaions.

It's not easy to buy it, and you must buy at least 2.000 pieces at once. this will be my annual requirements.

I hope, I can get some samples from NXP for my prototypes.

Once again: Thank You !!

Best regards,

Claus

0 项奖励
回复

3,342 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Claus,

There is no support on SW, but I attached some helpful libraries/driver examples.

Hope it helps.

Best regards,

Tomas

3,342 次查看
kerwinsun
Contributor II

I also look for the driver examples of UJA1076,you help me too.Thank you very much!

0 项奖励
回复

3,342 次查看
nikolayludov
Contributor I

Hi Tomas , can you help me with the software "uja 1168" or, for example, lib file or include file for C ?

0 项奖励
回复