SAHARA2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SAHARA2

2,926 Views
alexpan
Contributor I
I'm using iMX27. Is there any software example programs to teach me how to manipulate the SAHARA2 security co-processor? I'd like to be able to enable and disable it manually and have it to be transparent for end ueser's application.
Any assistance will be appreciated.
0 Kudos
Reply
2 Replies

1,773 Views
fabio_estevam
NXP Employee
NXP Employee
Yes, in the unit test programs there is a mxc_sahara_test directory that contains some examples.
 
You can do a ./ltib -c , then under Package list - - - > select [*] mxc-misc
 
To extract the sources: ./ltib -p mxc-misc -m prep
 
Then you can see the sahara examples at :
 
rootfs/unit_tests/mxc_sahara_test/
 
and the source at:
 
ltib-imx27ads-20071219/rpm/BUILD/misc/test/mxc_sahara_test
 
Regards,
 
Fabio Estevam
0 Kudos
Reply

1,772 Views
shashankpathak
Contributor II

Hi,

Can anyone suggest from where can i get the test programs?

Thanks,

Shashank.

0 Kudos
Reply