SAHARA2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SAHARA2

2,920件の閲覧回数
alexpan
Contributor I
I'm using iMX27. Is there any software example programs to teach me how to manipulate the SAHARA2 security co-processor? I'd like to be able to enable and disable it manually and have it to be transparent for end ueser's application.
Any assistance will be appreciated.
0 件の賞賛
返信
2 返答(返信)

1,767件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee
Yes, in the unit test programs there is a mxc_sahara_test directory that contains some examples.
 
You can do a ./ltib -c , then under Package list - - - > select [*] mxc-misc
 
To extract the sources: ./ltib -p mxc-misc -m prep
 
Then you can see the sahara examples at :
 
rootfs/unit_tests/mxc_sahara_test/
 
and the source at:
 
ltib-imx27ads-20071219/rpm/BUILD/misc/test/mxc_sahara_test
 
Regards,
 
Fabio Estevam
0 件の賞賛
返信

1,766件の閲覧回数
shashankpathak
Contributor II

Hi,

Can anyone suggest from where can i get the test programs?

Thanks,

Shashank.

0 件の賞賛
返信