SA604

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SA604

1,732件の閲覧回数
Santhibhushan
Contributor I

I would like to use SA604A for FM demodulation. I have FM modulated signal at 2.4MHz. Can i give directly to IF AMP -IN (pin-16) and then from IF AMP -OUT(pin-14) to pin-12 through 2.4MHz filter.

Can I get FM demodulated signal from pin-6 (audio out)? Also RSSI?

0 件の賞賛
返信
2 返答(返信)

1,726件の閲覧回数
LPP
NXP Employee
NXP Employee

FM signal at 2.4MHz can be demodulated using SA604A as described. Typical data rate is up to 100kbit/s.

Pin 7 (UNMUTE_AUD_OUTP) can be used for demodulated FM data stream. Pin 6 has similar function, but, it is more suitable for audio output since it support muting.

RSSI signal can be used to control the level of the input signal or to demodulate ASK signal.

Reference documents:
https://www.nxp.com/docs/en/application-note/AN1994.pdf
https://www.nxp.com/docs/en/application-note/AN1995.pdf
https://www.nxp.com/docs/en/application-note/AN1996.pdf
https://www.nxp.com/docs/en/application-note/AN1997.pdf
https://www.nxp.com/docs/en/application-note/AN1993.pdf

Best Regards,

Pavel

NXP TIC

 

 

0 件の賞賛
返信

1,719件の閲覧回数
Santhibhushan
Contributor I

Thanks for your reply and information.

0 件の賞賛
返信