SL3S1203_1213 Cannot read tamper alarm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SL3S1203_1213 Cannot read tamper alarm

1,061 Views
leo94
Contributor IV

I am using: 

  • Chip: SL3S1203_1213 UCODE G2iL and G2iL+,  
  • Reader: Impinj Reader Speeway revolution 420
  • Software:  Impinj Item Test .

From the documentation, i should be able to read the tamper bit with: 

Memory adress: Bank 01
Config Word , Bank adress: 200h Type: EPC, content:  tamper alarm flag initial 0b[2] remark: indicator bit

However i am only able to read the following: 

E2006B0700000000000000 , and nothing else. which doesn't look like a full EPC. 

I tried passing it: 

bit point (bit pointer in the software) =512 and lenght = 16 

still i only got back that EPC, and nothing else. 

 

 

Is there a problem with the chip? with the reader? the software? 

 

Following on from Reader for SL3S1203_1213 , how do i acutally pass these instructions through the software? 

I have also bought IMPINJ - Speedway R220 2-port, and IMPINJ SPEEDWAY CONNECT SOFTWARE, which should arrive in the next weeks. If the solution can be done with this software also this is great. 

 

 

 

 

 

0 Kudos
7 Replies

1,033 Views
leo94
Contributor IV

Hi Kan_Li since you updated the community and sent all the badge emails every NXP email went to spam ( just saw them 2 days ago) , this might have happend to other people too! 

I don't have access to that reader right now as it is in another department. But my reader (Speedway R220) with the software is coming in the following weeks, i'll update this post once i have that running). 

best, 

Leo

0 Kudos

1,019 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @leo94 ,

 

Thanks for the information! Please kindly let me know if the problem is still there.

 

Best Regards,

Kan

0 Kudos

986 Views
leo94
Contributor IV

Hi @Kan_Li ,

Have finally received the reader and installed, still having issues accesing the tamper bit: 

leo94_11-1603356158234.png

 

Let me know what parameters I need to change to access the bit 

Below are the screenshots of the settings on the speedway software, during my last attempt at trying to read the EPC:
 
 
leo94_0-1603356158191.png

 

 
 
 
leo94_1-1603356158196.png

 

 
 
leo94_2-1603356158201.png

 

leo94_3-1603356158206.png

 

 
 
 
leo94_4-1603356158209.png

 

 
 
leo94_5-1603356158213.png

 

leo94_6-1603356158216.png

 

leo94_7-1603356158219.png

 

leo94_8-1603356158224.png

 


 

 
 
Then i change status to on; apply; open putty with these settings:
 
leo94_10-1603356158231.png

 

 

 
 
thanks,
Leo 

 

 

0 Kudos

957 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @leo94 ,

 

Thanks for the information! 

From the screenshots , I would guess the reader expects the address in decimals here as it specifies “0 – 65535 bit in the brackets). Also, as with most readers it is more convenient to read the complete ConfigWord from the EPC memory and then “decode” this to get the value of the Tamper Alarm.

 

So, what I would advise here is to try and read the complete ConfigWord from the EPC memory with the according addresses, and the length of one word.

 

ConfigWord start address:

0x200h (bit address) == 0x20h (word address) == 32 (word address in dec)

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

952 Views
leo94
Contributor IV

Hi @Kan_Li , 

Thanks, we are now able to read the bit using word offset==32 as you suggested, 

However i still cannot get the whole EPC. Whilst using ItemTest i can only see the beginning digits, thus when i put 2 tags within the field, it only sees one. 

Below you can see 2 tags i put within the field: A has been cut (open tamper) B was cut and then attached again with silver Paste (closed tamper). However with both in the field it only reads one unique EPC and thinks there is only one tag. Then when i read the 32nd word i get sometimes the word for A, and sometimes the word for B

 
 

Item testItem test

 

0 Kudos

944 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @leo94 ,

 

Actually UCODE supports multiple tags reading, but it also depends on if the reader supports multiple tags , please kindly check with the reader vendor for further help.

 

Thanks for your patience and understanding!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,046 Views
Kan_Li
NXP TechSupport
NXP TechSupport
Hi Leo94, Do you have a snapshot of the settings in impinj reader software? We may help to check if your settings are correct. Thanks for your patience! Best Regards, Kan
0 Kudos