SA604

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SA604

1,726 Views
Santhibhushan
Contributor I

I would like to use SA604A for FM demodulation. I have FM modulated signal at 2.4MHz. Can i give directly to IF AMP -IN (pin-16) and then from IF AMP -OUT(pin-14) to pin-12 through 2.4MHz filter.

Can I get FM demodulated signal from pin-6 (audio out)? Also RSSI?

0 Kudos
Reply
2 Replies

1,720 Views
LPP
NXP Employee
NXP Employee

FM signal at 2.4MHz can be demodulated using SA604A as described. Typical data rate is up to 100kbit/s.

Pin 7 (UNMUTE_AUD_OUTP) can be used for demodulated FM data stream. Pin 6 has similar function, but, it is more suitable for audio output since it support muting.

RSSI signal can be used to control the level of the input signal or to demodulate ASK signal.

Reference documents:
https://www.nxp.com/docs/en/application-note/AN1994.pdf
https://www.nxp.com/docs/en/application-note/AN1995.pdf
https://www.nxp.com/docs/en/application-note/AN1996.pdf
https://www.nxp.com/docs/en/application-note/AN1997.pdf
https://www.nxp.com/docs/en/application-note/AN1993.pdf

Best Regards,

Pavel

NXP TIC

 

 

0 Kudos
Reply

1,713 Views
Santhibhushan
Contributor I

Thanks for your reply and information.

0 Kudos
Reply