hi,
We designed our own hardware board based on S32R45, Currently, pcie debugging encounters some problems, hope your help, thank you!
S32R45 SoC has two SerDes modules (0 and 1), each of them with one PCIe controller. Now, let me address the two main issues(only target at PCIE1 below):
1. Failed to stabilize PHY link(ssd card has been inserted)

2. The internal 100MHz reference clock could not be detected by oscilloscope.
Attention:
1. I configed pcie to RC mode.
2. we used R45 internal 100MHz reference clock.
3. uboot start command

4. linux pcie config

Otherwise, phy link nerver came up, primary cause may be 100MHz internal clock missing. From my perspective, R45 internal 100MHz(PCIE1_CLK_P/PCIE1_CLK_N) always exists after being powered on, why be gone.
Looking forward to your reply!