#S32R41 How to Debug I2c driver example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

#S32R41 How to Debug I2c driver example

1,988件の閲覧回数
hongweibai
Contributor I

I get two S32R41 M7_0 I2c examples from RTD Example, it  generates .bin and elf,but there is no QuadSPI reconfiguration data, How can  i get a qspi file without  QuadSPI reconfiguration data,Or is anyway to Debug  I2c example without qspi file

0 件の賞賛
返信
3 返答(返信)

1,968件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The question is a bit confusing, there is no relationship between the I2C debugging and QSPI reconfiguration data.

Could you please specify closer in details the issue?

Best regards,

Peter

0 件の賞賛
返信

1,963件の閲覧回数
hongweibai
Contributor I
Hello,So how to debug I2C example on M7_0,
I’m using Lauterbach Trace32 to debug it,I need .qspi file to execute S32R41_QSPI_flash_wrapper.cmm, then executing S32R41_CM7_0_attch.cmm to debug M7_0,but when I’m generating qspi file,there are some error.
Is there anyway to debug I2C Example on M7_0 with .bin and .elf file?
Thank you
0 件の賞賛
返信

1,924件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am still not sure if I understand you correctly.

But, yes, you can use precompiled binary files and load the to micro.

I dont know why you are not able to compile the code for QSPI.

You can use for example Trace scripts to load it directly:

petervlna_0-1708584577068.png

Best regards,

Peter

0 件の賞賛
返信