[S32R294] There is no Processor s32r294 in "Components Library".

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32R294] There is no Processor s32r294 in "Components Library".

1,455件の閲覧回数
Gordon_Yang
Contributor III

Hi,

I am a newbie at S32DS's IDE. I want to use the NXP's official SDK on S32R294.

After I updated "S32DS_PA_2.1_UP14.zip" for IDE and checked my "S32R294 development package" had been installed, there is still no "S32R294's Processor" in my "Components Library" -> "Processors".

How could I get "S32R294's Processor Components"?

Thanks.

Gordon_Yang_0-1616750679891.png

 

0 件の賞賛
返信
2 返答(返信)

1,406件の閲覧回数
Gordon_Yang
Contributor III

It seems that I re-install the SDK with the "default" path [i.e. C:/NXP] and this issue would be resolved. I don't actually know that whether it is the install path issue or the SDK link path setting issue. But I resolved this issue by this method.

0 件の賞賛
返信

1,438件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

it is in optional package for version S32DS v 3.4.

best regards,

Peter