S32 Design studio configtools warning

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design studio configtools warning

1,365 次查看
zhuoyue
Contributor I

When I used S32 design studio for S32 platform config S32G274A,the software configtoos appear same warning:

the power group VDD_IO_QSPI assign 1.8V, and VDD_IO_USB assign 1.8V ,the warning means :

the power group collision at "SIUL2_0", the power group should be assign different voltage,“VDD_IO_QSPI(4 properties)”. Then the config tools cannot update code. When I assign VDD_IO_QSPI and VDD_IO_USB 3.3V, the warning disappear.

But,the reference circuit board  QSPI power voltage is 1.8V  and  USB is 1.8V,I don't know why appear these warning ? Please help me solve this warning , thanks!

 

      

 

0 项奖励
回复
1 回复

1,345 次查看
bpe
NXP Employee
NXP Employee

All S32G documentation and software is currently under NDA. For this reason, NXP Technical Support cannot answer your questions in a public forum. To receive help with this issue please:

1. Register yourself on NXP Website with your corporate e-Mail account.

 

2. Open a Support Case.

 

Best Regards,
Platon/

0 项奖励
回复