Rotary Encoder Interfacing with PCAL9722

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Rotary Encoder Interfacing with PCAL9722

228 次查看
mk031
Contributor I

We are going to use Rotary incremental Encoder (Quadrature output) via SPI to IO Expander.

As Rotary Encoder requires Interrupt pin to interface, can you please Confirm whether it is possible to interface Rotary Encoder with PCAL9722 I/O Expander?

Does PCAL9722 supports interrupt on Rising as well as falling edge?

Thanks in advance!

0 项奖励
回复
1 回复

203 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Yes, the PCAL9722 supports interrupt functionality that can be configured by level or edge, and each interrupt can be cleared individually without affecting other interrupt events.

For more details, please refer to Section 6.4.12 – Interrupt Edge Registers (60h to 65h) in the datasheet.

Hope this helps!

 

 

0 项奖励
回复