Request for QSPI Slave Driver Support for iMX8 Lite OSM Module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Request for QSPI Slave Driver Support for iMX8 Lite OSM Module

1,266 次查看
Pooja_shetty
Contributor I

I am working on a project where we need to establish communication between an Achronix FPGA and an iMX8 OSM module using the QSPI interface. In our setup, the iMX8 Lite OSM module is configured as the master, and the FPGA is the QSPI slave.Is there an existing QSPI slave driver for the iMX8 OSM module? If so, could you provide the driver or point us to the appropriate resources?

Thanks & Regards,

Poojashree Shetty

标签 (1)
0 项奖励
回复
1 回复

1,221 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

I don't know about that module that you're using, I would suggest to contact your vendor and ask for this.

Even so, if they use the same driver we provide in their software package, then you may refer to ir here:
https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/drivers/spi/spi-fsl-qspi.c

Best regards/Saludos,
Aldo.

0 项奖励
回复